Road accidents involving single-person vehicles have become a significant concern in recent years. According to Injury Facts, a substantial percentage of fatal crashes involve a single vehicle, accounting for nearly 56% of all traffic fatalities in the United States. These accidents often occur due to blind spots, misjudgments while reversing, or obstacles that drivers fail to notice.
To address these issues, advanced automotive technologies, such as camera-enabled surround view systems, have been developed to enhance driver awareness and reduce accidents. Surround view systems provide a 360-degree view around the vehicle, significantly improving visibility and aiding drivers in making safer decisions. This technology is particularly beneficial for large trucks and cars, where blind spots are more pronounced and maneuvering in tight spaces can be challenging.
What are Surround View Systems?
Surround view systems are advanced automotive technologies designed to provide drivers with a comprehensive 360-degree view of their vehicle’s surroundings. These systems typically consist of multiple high-resolution cameras strategically positioned around the vehicle—usually on the front, rear, and sides.
The captured footage from these cameras is processed and combined to create a seamless bird’s-eye view. This enhanced view is then displayed on the vehicle’s dashboard screen. This technology is particularly beneficial for parking, reversing, and maneuvering in tight spaces. This is because it offers drivers a full perspective of potential obstacles that may not be visible through traditional mirrors or windows.
Advantages of Surround View Systems
Enhanced Safety: One of the primary advantages of surround view systems is the significant improvement in vehicle safety. By providing a real-time, all-around view, these systems help drivers detect obstacles, pedestrians, and other vehicles that could be in their blind spots. This enhanced visibility can prevent collisions and reduce the risk of accidents, especially in crowded or complex driving environments.
Easier Parking and Maneuvering: Parking in tight spaces and navigating through narrow streets can be challenging, even for experienced drivers. Surround view systems simplify these tasks by giving a clear, comprehensive view of the area around the vehicle. This helps drivers make precise movements and avoid minor collisions or scrapes that often occur during parking.
Reduced Blind Spots: Traditional mirrors and windows often leave blind spots that can be hazardous. Surround view systems effectively eliminate these blind spots by providing continuous, real-time visual coverage of the vehicle’s surroundings. This is particularly advantageous for large trucks and SUVs, where blind spots are more significant and harder to manage.
Improved Driver Confidence: With a better understanding of their vehicle’s surroundings, drivers can make more informed decisions. This not only enhances safety but also boosts driver confidence, making them more comfortable and reducing stress while driving.
Advanced Integration with Other Safety Systems: Surround view systems can be integrated with other advanced driver assistance systems (ADAS), such as automatic braking, lane departure warnings, and adaptive cruise control. This integration enhances overall vehicle safety and provides a more comprehensive approach to accident prevention.
Types of Vehicles Where Surround View Systems Are Used
Here are some of the primary types of vehicles where surround view systems are commonly employed:
Cars
In passenger cars, surround view systems significantly improve driver awareness and safety. They are particularly useful for parking and navigating in tight urban environments where visibility is often limited.
High-end and mid-range cars increasingly come equipped with these systems. They provide drivers with a bird’s-eye view to detect obstacles, pedestrians, and other vehicles. This technology helps prevent minor collisions and enhances overall driving confidence.
Smart Buses
Smart buses equipped with surround view systems benefit from enhanced safety, especially in urban settings where pedestrian and cyclist traffic is high. These systems assist bus drivers in monitoring blind spots, ensuring safer lane changes and turns.
Additionally, surround view systems help in navigating crowded bus depots and during parking. This reduces the risk of accidents and improves the overall efficiency of public transportation.
Related: How Embedded Vision is Helping Build Smart Buses of the Future
Autonomous Vehicles
Surround view systems are critical in autonomous vehicles, including delivery robots, autonomous tractors, and robot taxis. For delivery robots and autonomous tractors, these systems enable precise navigation and obstacle avoidance. This becomes crucial for operations in varied environments like urban areas or agricultural fields.
In robot taxis, surround view systems ensure passenger safety by providing comprehensive environmental awareness, thus aiding in safe navigation and stopping for pedestrians or other obstacles.
Cargo Trucks
Cargo trucks, due to their large size and significant blind spots, benefit greatly from surround view systems. These systems aid truck drivers in safe lane changes, reversing, and parking.
The enhanced visibility provided by surround view systems helps prevent accidents, especially in loading docks or when navigating through narrow roads. By improving situational awareness, these systems contribute to safer and more efficient freight transport.
Mining Trucks
Large trucks operate in challenging and often hazardous environments in the mining industry. Surround view systems are essential for these vehicles, providing drivers with a complete view of their surroundings.
This technology helps avoid collisions with other vehicles, equipment, or personnel. This in turn significantly enhances safety in mining operations. Moreover, in such high-stake environments, surround view systems aid in precise maneuvering, which is crucial for efficiently functioning mining activities.
Role of Embedded Cameras in Enabling Surround View
Embedded cameras are the cornerstone of surround view systems, playing a pivotal role in providing a comprehensive, real-time view of a vehicle’s surroundings. Typically, these systems utilize multiple high-resolution cameras placed strategically around the vehicle. Often, these cameras are equipped with fisheye lenses to maximize their field of view, capturing wide-angle footage that encompasses all potential blind spots.
Relevance of Multi-Camera Systems
Number of Cameras
The number of cameras required for an effective surround view system depends largely on the size and type of the vehicle. Generally, a minimum of four cameras is used—one at the front, one at the rear, and one on each side.
This configuration is usually sufficient for standard passenger cars. However, larger vehicles such as trucks, buses, and mining vehicles may require additional cameras to cover extended blind spots and provide a complete 360-degree view.
Field of View
The field of view (FOV) of each camera is another critical factor. Cameras with wide-angle lenses, often fisheye lenses, are typically used to maximize coverage. The FOV must be carefully selected to ensure overlap between adjacent cameras.
This is essential for stitching together a seamless surround view image. For larger vehicles, the FOV may need to be wider to cover more area and reduce blind spots effectively.
Processing Bandwidth
The processing platform’s bandwidth is a crucial consideration in a multi-camera system. Each camera generates a substantial amount of data that needs to be processed in real-time. The system must have sufficient processing power to handle this data without latency. Otherwise, this could compromise the effectiveness of the surround view system.
Resolution and Frame Rate
Camera resolution and frame rate are important for ensuring clear and detailed images. High-resolution cameras provide better image clarity. This is vital for detecting small obstacles or pedestrians. However, higher resolution also means more data to process.
Similarly, a high frame rate camera ensures smoother video, which is important for real-time applications where quick response is essential. The selected resolution and frame rate should balance clarity and processing capability to avoid overloading the system.
Frame Synchronization
In a surround view system, frames from multiple cameras are processed and merged to form a single image. It is important that frames are synchronized, which means that each camera begins and ends image capture at the same time. Without this, images from adjacent cameras may be exposed at different points in time. This requires the host processor to align the frames in time, and leads to excessive memory use and processor consumption.
For surround view applications, it is important to select a camera system that supports frame synchronization across multiple cameras, or even all cameras in a multi-camera setup.
Platform/Processor Compatibility
Compatibility between the cameras and the processing platform is essential. The cameras must be compatible with the vehicle’s onboard processing unit, which handles the integration and display of the surround view.
This includes ensuring that the communication protocols and data formats used by the cameras are supported by the processing unit. For example, if you are using GMSL2 or FPD-Link III cameras for your surround view system, a processor like NVIDIA Jetson AGX Xavier is well-suited.
Distance of Transmission
The distance over which camera signals need to be transmitted can affect the choice of cameras and cabling. Longer transmission distances can introduce latency and signal degradation.
This must, however, be minimized to maintain image quality and real-time processing. High-quality cables and signal amplifiers may be necessary for larger vehicles. This ensures that the data from cameras positioned far from the processing unit remains intact.
Add link to GMSL2 cameras here.
TechNexion – High-quality Cameras for Surround-view Systems
TechNexion has a wide range of cameras suitable for surround view systems in its portfolio. We offer multi-camera solutions compatible with processors like NVIDIA Jetson and TI TDA4VM. These high-end cameras are ideal for robots, buses, trucks, autonomous tractors, and other vehicles requiring surround view. Contact us to learn more about how our cutting-edge camera solutions can meet your imaging needs.
Related Products
Get a Quote
Fill out the details below and one of our representatives will contact you shortly.