Quicker backup of SD cards

Difficulty Levels: Intermediate
Date added: July 6, 2018
Affected Products: BLIZZARD , EDM-GNOME , EDM-IMX7 , EDM1-FAIRY , EDM1-GOBLIN , EDM2-ELF , EDM2-GREMLIN , PICO-DWARF , PICO-HOBBIT , PICO-IMX6 , PICO-IMX6UL-NAND , PICO-IMX6UL-NOR , PICO-IMX7 , PICO-NYMPH , TC-0700 , TC-0710 , TC-1010 , TEK3-IMX6 , TEK3-IMX6UL , TEP-0500-IMX6UL , TEP-0500-IMX7 , TEP-0700-IMX6UL , TEP-0700-IMX7 , TEP-1010-BSW , TEP-1560-BSW , THB-3517 , THUNDER , TSUNAMI , TWISTER , TWP-1010-IMX6 , TWP-1560-IMX6 , WBDUAL , WBQUAD , WBSOLO

Introdction

This article shows a script that copies an SD card to hard drive using efficient reading and minimizing the amount of data read.

The ideas are two: only copy the area that is used (i.e. partitioned with non-swap partitions), and do the reads in larger chunks than the typical erase block.

Using fdisk -lcu /dev/sdX the partitions are listed in number of sectors of 512 bytes. Naively reading a large count of 512 byte blocks in a dd command could lead to a many small reads and be potentially very inefficient. Instead the script uses the following observation: reading N blocks of 512 bytes, equals reading 512 blocks of N bytes. It is perfectly possible to swap the block size and the count parameters in a dd command.

Script

The script is as below. It takes two arguments: block device of the sd card and the filename for the copied SD card image.

#!/bin/sh

dev=$1
outfile=$2
if [ X$dev = X ] || [ Y$outfile = Y ]
then
        echo Usage : $0 device filename
        exit
fi

devminor=`basename $dev`
bs=`echo pq | fdisk -u $dev | grep -v 'swap' | grep $devminor | tail -1 | awk '{print $3 }'`
bs=`expr $bs + 1`
dd if=$dev of=$outfile bs=$bs count=512 2>&1 > /dev/null

Stay up to date with all the latest TechNexion news...

Sign-up for our Newsletter