Home
Solutions
Solutions Fanless
Benefits
- true silent operation.
- optional waterproof and dustproof sealing for operation in harsh environments.
By using TechNexion's fanless products that can be sealed to waterproof/dustproof standards like NEMA 4/4X and IP65 can you deploy systems in every possible thinkable environment.
There are actually different ways to achieve fanless operation.
1. Using ULV (ultra low voltage) components. By using components that have a minimal power consumption you tackle the problem right at the point where it is coming from. Powerconsumption in computer systems is sooner or later converted into heat. The less power consumption. The less heat development.
2. Using convection cooling. This can be done by having a relative large internal volume in a computer unit that allows air to float freely.
3. Using heatpipes and heatsinks. This technology is used together with ULV and LV (low voltage) components. The principle of this technology is that you use heatpipes connected on one side to the heated components (such as the processor and core chipsets). On the other side you connect these heatpipes to heatsinks that are either embedded in the chassis or are part of the exterior of the chassis. The technology works as follow. The heatpipe is like an "expressway with the two ends connected to the heatsource and the heatsink. The heatpipe just want the temperature everywhere to be the same. Which means in reality that it is transporting heat from the heatsource towards the heatsinks.
TechNexion has experience in emplementing all above technologies and based on the designated project we can propose the best working solution to you.
For your reference you can find our standard fanless products below.
Related Products
- Box Computer

TESSA-LX
Fanless small formfactor embedded controller featuring AMD LX800 microprocessor.
- Power Supply

PS-DC-ATX-60W
60 Watt DC to ATX converter board.
PS-DC-ATX-80W
80 Watt power converter board.
PS-DC-ATX-120W
120 Watt DC converter board.
PS-DC-ATX-125W
125 Watt DC converter board.
PS-DC-ATX-200W
200 Watt DC converter board.