TechNexion annouces its participation in NXP’s Early Access Partner program for the new NXP i.MX8M applications processor

Through its participation in the program, TechNexion will collaborate with NXP to further accelerate time-to-market of next generation processor family.

TechNexion today announces its inclusion in NXP’s Early Access Partner. Having met the program criteria, TechNexion has been selected to participate in NXP’s Early Access Partner program for the next generation i.MX8M applications processor family. The inclusion in this program will translate into shorter time-to-market for TechNexion’s customers.

The NXP i.MX8M family of application processors based on ARM Cortex-A53 and Cortex-M4 cores provide industry-leading audio, voice and video processing for applications that scale from consumer home audio to industrial building automation and mobile computers. The NXP i.MX8M processors family has up to four 1.5 GHz ARM Cortex-A53 and Cortex-M4 cores, high-speed connectivity interfaces and flexible memory options. The processors also feature full 4K UltraHD resolution and HDR video quality, the highest levels of pro audio fidelity, up to 20 audio channels and DSD512 audio. The i.MX8M family includes the i.MX8M Solo, i.MX8M Dual, i.MX8M QuadLite and i.MX8M Quad.

TechNexion’s portfolio of products based on the NXP i.MX8M processor, will include a complete lineup of System on Modules designed for modular, versatile, scalable and power-efficient applications. The modules are expected to be available in fourth quarter of 2017.

About NXP Semiconductors

NXP Semiconductors enables secure connections and infrastructure for a smarter world, advancing solutions that make lives easier, better and safer. As the world leader in secure connectivity solutions for embedded applications, NXP is driving innovation in the secure connected vehicle, end-to-end security & privacy and smart connected solutions markets. NXP invests in research and development so it can provide some of the highest-performing, richly-optimized, smallest-geometry products. Built on more than 60 years of combined experience and expertise, the company has 45,000 employees in more than 35 countries.

About TechNexion

TechNexion offers a wide range of embedded modular solutions to leading OEM/ODM companies in the multimedia, communication, security, automation and process control industries. TechNexion continuous investment in production technology and state-of-the-art equipment upgrades make it possible to meet technically increasingly complex customer demand. TechNexion products range from Systems on Module, Embedded Mainboards, Fanless Computing, Panel Computing to Internet of Things. All products and solutions are backed up with unmatched longevity, open hardware documentation and open source software.

TechNexion is a ISO-9001 and ISO-14001 certified company and is a founding member of the EDM (Embedded Design Modules) Standard.
For more information, visit www.technexion.com.

Stay up to date with all the latest TechNexion news...

Sign-up for our Newsletter